专业知识

A Century of Aerospace Innovation

自从飞机、直升机、宇宙飞船和卫星诞生以来,航空航天工程师就一直向铁姆肯公司寻求减少摩擦的解决方案。 任何设计用于飞行的机器都需要坚固、高效的轴承,能够承受极端条件并在危急情况下可靠运行。

如今,铁姆肯公司工程师正在与世界各地的航空航天合作伙伴合作,设想、开发和生产 21 世纪的飞行器。 他们正在设计效率更高的下一代直升机;与美国宇航局合作开发“蜻蜓”旋翼机,该旋翼机将探索土星的卫星泰坦;并对将改变城市的电动垂直起降出租车进行微调。

从莱特飞行器到韦伯望远镜,了解铁姆肯公司团队在过去几十年中如何帮助解决关键的航空航天挑战。

  • 1903
  • 1930s
  • Mid-1930s
  • 1935
  • 1940s
  • 1953
  • 1964
  • 1969
  • 1996
  • 2003
  • 2009
  • 2012
  • 2020
  • Feb. 2021
  • Dec. 2021
  • 2023
  • Oct. 2024
  • Earthbound No More

    Using Diamond® chain products from their bicycle shop, Orville & Wilbur Wright pioneer the era of aviation with the world’s first manned, controlled flight near Kitty Hawk, North Carolina.

  • Ubiquitous Durability

    Timken is the go-to supplier as the World War II Allies look for robust, rugged, durable bearing solutions. Each B-17 Flying Fortress uses 240 Timken bearings.

  • Super Steel Changes the Game

    Timken metallurgist Martin Fleischmann patents a corrosion-resistant steel alloy which leads to Super Steel 16-25-6 — an alloy giving Allied bombers and fighter planes critical advantages in the final stages of World War II. Super Steel is also essential in the development of postwar turbojet engines.

  • A Revolution in Commercial Air Travel

    Timken® bearings in the Douglas DC-3 make commercial air travel comfortable, reliable and profitable.

  • Bringing a Lifesaving Dream to Life

    Timken engineers work closely with Igor Sikorsky to develop the R-4 — the first helicopter to be sold in high volume. Its ability to hover as well as fly up, down and sideways make it ideal for lifesaving missions.

  • Air Travel Upgrade

    Twenty Timken® bearings — used in both the propellers and landing wheels — support the British Vickers Viscount, the first turboprop airliner — known for its smooth, quiet ride, panoramic windows and low operational costs.

  • Mach 3 Speeds

    Longtime partner, B.F. Goodrich designs Timken® bearing into the landing gear of the Lockheed SR-71 Blackbird US Air Force reconnaissance plane. Built to fly above Mach 3 (three times the speed of sound), its 1976 airspeed record for air-breathing flight — 2,193.2 mph — still stands.

  • Guiding the First Moon Walkers

    Timken’s work on inertial guidance systems bears fruit in Apollo 11’s Lunar Exploration Module, guiding astronauts to the moon for the first time. The same system is used in 1970’s Apollo 13 to guide astronauts back to Earth after the main guidance system fails.

  • Exploring Mars: Pathfinder

    Timken® miniature, precision bearings play a critical role in the Pathfinder mission, which lands Sojourner, the first rover to explore the Red Planet.

  • Exploring Mars: Spirit and Opportunity

    NASA’s “twin robot geologists,” Spirit and Opportunity rovers, rely on Timken bearings for their descent to Mars.

    Play Video

  • Meeting the Extreme Challenges of Space

    Astronauts embark on a spacewalk to make delicate repairs to the 30-year-old Hubble Space Telescope. To withstand the extreme operating temps and vacuum of space, the mini power tools they carry use a custom thin-section precision ball bearing designed by Timken engineers.

  • Exploring Mars: Curiosity

    In addition to using Timken® bearings in its descent, the Curiosity rover also has Timken® bearings in the center hub of its sample carousel system. Two ¼ inch (6.35 mm) Timken® bearings also run the tiny vacuum pump that supports the rover’s analytical equipment.

    Play Video

  • Covid-19 Disrupts Air Travel

    When thousands of passenger jets are grounded during the Covid-19 pandemic, the all-important landing wheel bearings sit quiet — a state they were never designed for — Timken service engineers step in to develop maintenance and inspection procedures so aircraft can return to service quickly and safely when the time comes.

  • Exploring Mars: Perseverance

    GGB, a Timken brand, partners with NASA to develop tribological solutions used in the sampling and caching systems of the Perseverance Rover which lands on Mars in search of signs of ancient life.

  • Peering Into Infinity

    Supported with Timken technology, The James Webb Space Telescope launches a new era of deep space exploration. Timken bearings are used in two critical systems: Mechanisms that secure key components of the space telescope prior to deployment, and the downlink antenna that makes communication possible.

  • Next-Level Efficiency

    Timken launches a complete line of tapered and cylindrical bearings featuring silicon nitride (ceramic) rollers. The hybrid bearings are lighter, stronger, and more efficient than all-steel bearings — perfect for extreme aerospace requirements.

  • NASA launches Europa Clipper

    NASA recently launched the Europa Clipper, a robotic, solar-powered spacecraft built to orbit Jupiter and capture high-resolution images of Europa, one of its four largest moons. Scientists will use the images to understand Europa’s icy shell, determine if the ocean beneath it could support life and identify sites for future landing missions.

    High-precision, preloaded stainless thin-section bearing pairs from Timken support the camera system mounted on the outside of the spacecraft — with minimal protection from the temperature and radiation extremes it will encounter on its multi-year flight.

    Follow the Europa Clipper’s progress at NASA.

“世界上大多数飞机都依靠铁姆肯公司起落轮轴承起降。每年数十亿人的生命依赖于这个关键部件,该部件每天必须多次承受极端条件。”

保罗·伊森
航空工程师

“客户相信我们的轴承专业知识可以帮助他们探索太空、发现宇宙,甚至跟踪和预测天气。”

斯科特·拉法拉姆
应用工程专家

“铁姆肯公司的耐磨、热管理、高速、功率密集、高负载产品完全符合飞机设计师的需求。”

博士。瑞恩·埃文斯
研究与开发总监

当我们迈向未来时,有一件事是明确的:航空航天的突破将永远是社区的努力——将不同文化和空间的人们聚集在一起,相互学习,让最困难的挑战看起来很容易。