The Timken Company acts responsibly, exercising sound judgment in our dealings in accordance with our ethical standards and the law. On August 22, 2012, the U.S. Securities and Exchange Commission issued the conflict minerals rules (the “Rules”) under Section 1502 of the Dodd-Frank Wall Street Reform and Consumer Protection Act of 2010. The Rules require reporting and disclosure of the use of conflict minerals in the products of publicly traded companies. The law and the Rules were enacted in response to reported human rights violations and armed conflicts in the Democratic Republic of the Congo and its surrounding countries (the “DRC region”). Under the Rules, conflict minerals are defined as tin, tantalum, tungsten and gold (“3TG”).
Most of Timken’s products do not intentionally contain 3TG. Our core products are made from recycled scrap steel. To the extent 3TG is used, Timken is committed to responsibly source such 3TG. Nie będziemy świadomie zapewniać korzyści ani finansowania grupom zbrojnym zaangażowanym w bezprawny konflikt w regionie DRK. We will conduct the necessary inquiries and due diligence on the source of the 3TG that is used in our products. We expect our suppliers to hold themselves to the same standards. We will work with our supply base to source from 3TG upstream suppliers, smelters and refiners that do not contribute to the violence in the DRC region. Suppliers are also required to comply with Timken’s annual conflict minerals reporting requirements, which are designed to provide Timken with the information we need to make responsible sourcing decisions.
Formularz SD i raport dotyczący minerałów z regionów ogarniętych konfliktami